3/16/2017 4:09 PM | |
Posts: 2 Rating: (0) |
we are using MM420 before, but now we want to change it to MM440 and we are facing a problem of output frequency from the drive. We are using profibus for the communication through monitor (PC). but, the problem now is that when the speed of the electric motor is set to 100 from the monitor (PC) it will be showing 50 on the drive BOP and the speed of the motor will slow. Please what is the way out i mean is that when the speed on 100Hz from the monitor through profibus the drive will display 50Hz on the BOP and the motor will be running at 50Hz ------------------------------------------------------------------------------------------ |
Last edited by: bolah at: 3/17/2017 7:38:22 AMLast edited by: Min_Moderator at: 3/17/2017 2:18:04 PMNew subject after splitting |
|
Follow us on