3/19/2017 3:56 PM | |
Posts: 1 Rating: (0) |
Hello, I have connected the RTD (Pt100) on 6ES7331-1KF01-0AB0 at channnel 3 and analog reading is (integer) 10 while the actual temperature is 24oC. if i get the actual value then it will be divided by 10 to obtain the actual temperature.Can any one tell me where the problem is?? or is it better to add offset of 14 to obtain the actual temperature. Settings are below temp : oC Freq:50Hz RTD Pt100 std i'll be thankful if anyone can help Thank you. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 3/20/2017 4:24:00 PMNew subject after splitting |
|
Follow us on