Industry Online Support
Technical Forum
3/23/2017 1:26 PM | |
Posts: 1 Rating: (1) |
Hi, I am doing the modular testing of gas turbine, so for that i need to record some particular set of IOs. I am using the PLCSIM S7-1500 for the testing. Is there any tool for Tia portal which is similar to data logging in RXLogix 5000, where I can continuously record selected variables. I tired the same with the Trace Functionality, and it has two limitations, 1. More than 16 variables cannot be recorded 2. Cannot record more than a particular period of time (Depends on the sampling time). Can you suggest a suitable method for the same? Can we log data using OPC? Thanks & Regards Manuprasad S N ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 3/23/2017 4:02:13 PMNew subject after splitting |
|
Follow us on