4/11/2017 3:08 AM | |
Posts: 31 Rating: (0) |
On the screenshot 2 shows simple programs on each PLCs |
4/11/2017 3:09 AM | |
Posts: 31 Rating: (0) |
On the screenshot 3 shows tags in HMI Panel |
4/11/2017 3:13 AM | |
Posts: 31 Rating: (0) |
On the screenshot 4 shows statuses of simulators. After pressing button on HMI rectangle must change color |
4/12/2017 2:07 AM | |
Posts: 31 Rating: (0) |
PLCSIM of 1515 CPU has bug? PLCSIM of 1200 and 300 CPUs work fine. Video attached |
4/12/2017 7:50 AM | |
Joined: 8/3/2009 Last visit: 9/27/2024 Posts: 13803 Rating: (1741)
|
Hello CDrom I´m not sure if you have a Basic Panel 1st or 2nd generation. Look in this FAQ: https://support.industry.siemens.com/cs/de/en/view/109742764 The fact is that a basic Panel 1st generation has only a V12 Image. No newer one is available! And you need at least V14 Image for HMI to get the Simulation with PLCSim V14 (S71200/1500) run. If you have a Basic Panel 2nd Generation or Comfort Panel just update the Image as described in the FAQ. Have a nice day Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
4/13/2017 1:16 AM | |
Posts: 31 Rating: (0) |
Very well, but for KP400 Basic Panel change version to 14 not possible. TIA has no version 14 for this panel. |
Follow us on