4/28/2017 10:54 AM | |
Posts: 25 Rating:
|
Hii, I am using analog pin A0 of Arduino to read a sensor value. I successfully read and print the sensor value in serial monitor using arduino ide. Now I need to read the same using python code. For that I should know the pin number to which A0 is connected to intel quark processor. Can anyone help me in finding this. Also in the python code what all packages are to be imported. Thanks in advance ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/2/2017 10:48:10 AMNew subject after splitting |
|
4/28/2017 11:27 AM | |
Posts: 4 Rating:
|
To use the analog ports with python you can use the mraa toolkit: https://github.com/intel-iot-devkit/mraa There is a example for the analog port: https://github.com/intel-iot-devkit/mraa/blob/master/examples/python/aio.py |
This contribution was helpful to
1 thankful Users |
Follow us on