5/3/2017 2:09 AM | |
Joined: 9/1/2015 Last visit: 8/31/2024 Posts: 13 Rating: (1) |
Hi! I need to buy a M5 Field PG + Scout License. I have two machines, one of them programmed whith Scout (under Step7 V5.5) and the other one with Scout TIA V13. I prefeer not to migrate the program to TIA envirorment, so: Is it correct if I buy a PG with "STEP 7 & WinCC Combo: STEP 7 Prof. Combo (V14 & 2010), WinCC Adv. Combo (V14 & flex. 2008)" and a "SIMOTION SCOUT V4.4 HF2 Engineering System, incl. SCOUT TIA, on DVD with full license" (6AU1810-1BA44-0XA0) to support both machines? Thanks in advanced!! ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/4/2017 2:33:03 PMNew subject after splitting |
|
Follow us on