5/11/2017 5:19 PM | |
Joined: 5/4/2016 Last visit: 7/25/2023 Posts: 4 Rating: (1) |
Hello people, I'm having a strange problem when I try to archive/disarchive project in my laptop: - if the compressed project is in two subfolder level from theroot level of my hard drive, I fail to archive/disarchive: "error number 3020:46" when disarchive; no error when create the archive but the file is not present in the target path; - if the compressed project is in one subfolder level in my drive all works properly. These are the conditions that I have been checked: - My login account is a member of administrator of the machine; - I give to user "Everyone" the full control in the security settings of the main folder; - I tried to disable the antivirus protection (Eset Smart Security 10); - I set the "8dot3" property to "Enable" for all the volume, - I tried to repair the installation with the DVD; - I tried to create a new folder from the disk root and a subfolder inside and the result is the same; OS is Windows 7 Pro SP1 x64 with Step 7 Pro 5.5 SP4. Thanks!
------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/12/2017 2:43:05 PMNew subject after splitting |
|
Follow us on