6/8/2017 8:15 AM | |
Joined: 4/28/2015 Last visit: 4/5/2024 Posts: 66 Rating: (4) |
Good day for all! I have the similar problem with PLCSIM v14 SP1 Upd1. When i tried to start simulator alone, without starting TIA portal i had the crashreport with "simatic.plcsim.vplchost problem". I tried to uninnstall PLCSIM v14, delete folder PLCSIM V14 in ProgramData. Then i reinstalled PLCSIM V14 SP1 and then added upd1. But it still not working. I use win7 64bit. I have both TIA V13 and TIA V14. With TIA V13 i have no any problem. I readed about the similar problem for v13 sp1. S7-PLCSIM v13 SP1 crashes on creating project There was file for repairation registry, may be somebody knows how to fix problem with v14? Thanks. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 6/8/2017 1:21:26 PMNew subject after splitting |
|
Follow us on