10/1/2015 5:06 PM | |
Posts: 439 Rating: (108) |
Hi Stas, https://support.industry.siemens.com/cs/us/en/pv/6ES7523-1BL00-0AA0/td I don't know your timer, but you tell that the timer is able to supply up to 2A. It does not mean there will be 2A. You should give more information about your timer. If it's a timer relay than it is basically a contact that close when the timer is finish. So the current is related to the charge which is the input of the DI/DQ. The input have 20mA current consumption, so your timer is ok with it's 2A.
Best regards, Hugo |
Follow us on