6/28/2017 1:04 PM | |
Posts: 64 Rating: (7) |
Hi smiffy, I am trying to make a model in the library and create replicas of it, I have put two process tags (a valve and an analogue monitor) and a picture into a library hierarchy folder and defined it as a model. The CFCs work fine, but I have some questions about how to best deal with the picture: Is there a way to define the name of a picture in the replica during the model import? As it is now, it just takes the picture name from the model and appends a number in brackets to it, but I would like to have the pictures named after their P&ID diagram. Is there a way to automatically generate block icons in the library picture? (for example, if I can define in the model that the valve and monitor go certain places in the pictures, their (project) PTs go to the same places in the picture of the replica? Thanks in advance. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 6/29/2017 12:33:46 PMNew subject after splitting |
|
Follow us on