6/30/2017 11:18 AM | |
Posts: 40 Rating: (0) |
HI SAME PROBLEM. CONTROL PANEL INFEED I can not mark p864 BI: Infeed operation Control_Unit : r722.0 Ready to run 2 OK p210 Drive unit line supply voltage 600 V Ready to run 3 1 63000 OK MERHABA AYNI SORUNU YASIYORUM. CONTROL PANEL UZERINDEN MOTORA HARICI CONTROL YAPMAK ISTEDIGIMDE HAT KONTAKTORU ACIYOR. CONTROL PANEL UZERINDEKI INFEED SECIMINI YAPAMIYORUM
------------------------------------------------------------------------------------------ |
Last edited by: izzetguleser at: 6/30/2017 11:19:51 AMLast edited by: Jen_Moderator at: 7/3/2017 11:12:38 AMNew subject after splitting |
|
6/30/2017 11:26 AM | |
Joined: 5/12/2006 Last visit: 7/25/2024 Posts: 22324 Rating: (2999)
|
which line module you use? is it connected to the same CU like the motormodule? |
Follow us on