7/7/2017 12:54 PM | |
Joined: 4/29/2016 Last visit: 5/19/2024 Posts: 30 Rating: (1) |
hello H.J. I done it , with the help of link given by you before one year at the time of commissioning. But, now further one problem has arise now , when i had to format my PC due to OS crashed. After format my PC i had to install WinCC Advanced Runtime V12 only, i installed it and activate Runtime Backup.Plant is running . But, Due to PC format SQL Server 2008 have to install further, also. But after installing SQL Server 2008 i can not connect with wincc server because i don't find "PC-NAME\\WINCCPlus" Server name in dialogue box in SQL Server management studio. Not only that , but i don't find any others of server name. Before Format PC , I had done Database creation in SQL server and as well as define Database name in with same name defined in SQL As per link guidance. and all was well, But issue raised after format PC. help me. it's urgent. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 7/11/2017 2:03:53 PMNew subject after splitting |
|
Follow us on