7/13/2017 12:58 PM | |
Posts: 3 Rating: (0) |
Hello, I have a similar Problem. I connected a Thermocouple Type K to the Signal Board TC Input and have a 12Deg Celsius inaccurate Reading of Temperature. (Dividing by 10x is not the problem) It's just very inaccurate. I changed already the sensor and nothing improved. same inaccuracy. The source reference Temperature is set to Internal Reference. Does this say I need to do any offset with 0 or 20Deg etc? Please help. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 7/13/2017 1:31:02 PMNew subject after splitting |
|
7/17/2017 4:15 PM | |
Joined: 7/7/2010 Last visit: 4/26/2024 Posts: 14639 Rating: (2349)
|
If you connect the TC using proper TC cable for Type K TC's directly to that signal board, does it read correctly? Well, IW80 = actual temp x 10 as you already stated. Does IW80 read properly then?
|
science guy |
|
Follow us on