7/19/2017 12:33 PM | |
Posts: 1 Rating: (0) |
Hi! I'm receiving this error on one pc (henceforth we will call PC-A) after cloning. What happened was after a power failure, the original hard disk of PC-A got corrupted (by some luck of the UPS failing). So the solution that i thought of was to make a clone of one of the other PCs (henceforth we will call PC-B). PC-A (cloned hard disk) will boot up and will be open the wincc project in runtime but it was "sharing" communication with PC-B. When PC-A is active PC-B is inactive and vice versa. Then i thought of changing the pc name (in wincc explorer and computer properties) and ip address (in the tcp/ip properties) but after i would see the database contextdoes not exist or is invalid error. I tried what mr.Rafal suggested bu still doesnt work. I'm running wincc ver6.2 on a windows xp system by the way and i dont have a solid understanding of scada systems yet. I hope somebody can help me out... ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 7/27/2017 7:25:33 AMNew subject after splitting |
|
7/27/2017 4:29 PM | |
Joined: 5/13/2008 Last visit: 12/18/2019 Posts: 836 Rating: (71)
|
Hi, please find additional informations about changing the computer name after installation of SQL: What restrictions are there for assigning the computer name for WinCC? |
mfG / Best regards |
|
Follow us on