8/11/2017 9:36 AM | |
Posts: 6 Rating: (0) |
Hello friends, I`m new in industrial PC and soft PLC, so I got big problems. I have IPC427D (6AG4140-4BL04-4AN0), with WinLC RTX V4.6.2 (6ES7611-4FB00-0YB7) integrated, so I need help like for beginners how to set HW config in TIA V13, by that i mean if that microbox IPC427D have 2 ethernet port and one MPI, how do i create in tia portal V13 that - I did insert from HW catalog IPC427D - validated version, and do i need to put OPC in slot? and how to wire WinLC RTX F with onboard ethernet port... I would appreciate if you would help the newbie like me, thank you. nice greetings, Cwika ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 8/11/2017 10:33:42 AMNew subject after splitting |
|
8/11/2017 11:41 AM | |
Posts: 6 Rating: (0) |
Hello Cristoph, thank you for fast replay, I did everything like you said, but still got some errors more in picture. Thank you, Cwika AttachmentAAAAAAAAAAA.zip (847 Downloads) |
8/11/2017 11:49 AM | |
Joined: 5/12/2006 Last visit: 4/25/2024 Posts: 22227 Rating: (2980) |
click on the blue "?" sign to get information what is wrong with the configuration |
8/11/2017 1:12 PM | |
Posts: 6 Rating: (0) |
Here it is, but I had some Fail Safe blocks in it now I lost it, can u tell me how can I make it back? |
8/11/2017 2:03 PM | |
Posts: 6 Rating: (0) |
Hi, didnt create back up, but nvm. I dont have exp with IPC and softPLC, do I need to configure something on IPC in Station configurator? Pictures in attachment. Cwika AttachmentPics.zip (693 Downloads) |
8/11/2017 2:21 PM | |
Joined: 5/12/2006 Last visit: 4/25/2024 Posts: 22227 Rating: (2980) |
Hi, the configuration of the Station Configurator look ok, no changes need here. Regards |
Follow us on