(0)| 8/11/2017 7:33 PM | |
|
Posts: 6 Rating:
|
hi , i cant seem to connect to my s7-300 , 6fc5 317-2fk14-0ab0, firmware 3.2.10 cpu - 317f-3 pn/dp i have just pinged all , the control module ( which im in right now) and the 2 plcs, ) i have tried connecting ethernet into the spare port on the plc (bottom one) and tried into the control module trying anything really. i can see them all in the accessable nodes, i can ping them, ive setup my ip on computer as xxx.xxx.214.50 - computer subnet 255.255.255.0 gateway - xxx.xxx.214.1 ( tried all of them) xxx.xxx.214.1 - control module xxx.xxx.214.4 - top plc xxx.xxx.214.5 - bottom plc im just out of ideas. the plcs dont have serial connection , only ethernet ( which has 2 each 1 has profinet jumpering them to each other.) ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 8/14/2017 10:55:23 AMNew subject after splitting |
|
Follow us on