9/12/2017 10:06 AM | |
Posts: 305 Rating: (2) |
1512SP via PN connect 14 NUM V90 PN . CONFIG, 1500 HAS 10 POSITON AXIS , NOW , I THINK USE FB284 TO CONTROL 14 AXIS ,is it OK ? my system is ptp motion ... |
9/12/2017 11:19 AM | |
Posts: 305 Rating: (2) |
how many SINA_POS can control aixs ? IRT time is 4ms,1512 can control 14 axis to PTP motion ? |
Last edited by: TechWing at: 9/12/2017 11:20:46 AM |
|
9/12/2017 8:22 PM | |
Joined: 5/22/2012 Last visit: 3/24/2022 Posts: 895 Rating: (67) |
... for SINA_POS and basic positioner you don´t need IRT- communication. |
1/29/2018 12:50 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by Tamizh2007 is split to a separate thread with the subject V90 F31101 fault . Best regards |
Follow us on