9/14/2017 3:31 PM | |
Posts: 1 Rating: (0) |
Does anyone know the accuracy of the clock memory byte CPU1212C DC/DC/DC? I have a program I am looking at improving and it bases calculations on the 1 Hz clock. The calculations are quite time sensitive and I am concerned that I may need to directly access the real time clock instead. However, if the real time clock is tied to the clock memory byte then I would just like to know its accuracy to specify this in the tolerances. Thanks, ------------------------------------------------------------------------------------------ |
Last edited by: Paul_S_Barker at: 9/14/2017 3:39:10 PMLast edited by: Jen_Moderator at: 9/15/2017 12:21:27 PMNew subject after splitting |
|
Follow us on