11/16/2017 6:58 AM | |
Joined: 9/2/2012 Last visit: 7/17/2024 Posts: 711 Rating: (30) |
Dear JoshMayer, we are also facing the same issue with "6ES7132-6BH00-0BA0" card. it was conncted to LED lamp, so because of this 7v issue, its started to glow. without load, across multi-meter it shows 7v. Contacted hotline and they have replied that, "this is a voltage caused by the integrated broken circuit detection of the module. Does anybody having basic card to check the voltage is coming or not ? |
Last edited by: Jen_Moderator at: 11/16/2017 1:04:33 PMNew subject after splitting Last edited by: Jen_Moderator at: 11/17/2017 1:11:00 PMDeleted splitting remark.
|
|
11/17/2017 1:01 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1052) |
hi vipz, wirebreak-diagnostic can be disabled with the DQ-module that you have SIMATIC ET 200SP Digital Output Module DQ 16x24VDC/0.5A ST hope this helps, regards, |
Last edited by: Jen_Moderator at: 11/17/2017 1:12:19 PMAdded picture as an attachment. FCK WAR! |
|
Follow us on