10/24/2017 9:12 AM | |
Posts: 14 Rating: (1) |
Hello, I have a question about the 4th question. It is impossible to reach the function "ShowPopupScreen" from within a faceplate. Therefore I cannot make a [X] to close the pop-up. This workaround doesn't feel very elegant. Is there a better way? Best Regards ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/25/2017 8:31:57 AMNew subject after splitting |
|
10/26/2017 10:25 AM | |
Posts: 14 Rating: (1) |
I found the solution Set Event on the faceplate itself with the function showpopupmenu with displaymode either Toggle or OFF. Inside of the faceplate you need to open the interface menu and select events. From here you can link the event from the button to the outside event on the faceplate. |
This contribution was helpful to4 thankful Users |
Follow us on