10/25/2017 10:56 AM | |
Posts: 14 Rating: (6) |
Hi Kiiza the APL Style Guide provides the information, design specifications and rules that you require to adapt project-specific blocks in conformance with APL. You will receive support in these required adaptations by examples of actions. APL Style Guide: The APL Operator Guide supports you in operating the APL block icons and faceplates. It offers information about the numerous displays, operator control functions and graphs, which you can use in your daily work. APL Operator Guide: Hope this helps. Regards |
10/25/2017 1:28 PM | |
Joined: 3/14/2008 Last visit: 9/23/2024 Posts: 2096 Rating: (938)
|
Hello Saarlodri, The APL library is only used as of PCS7 V7.1. In PCS7 V7.0, the classic library is used. @Kiiza: See the following manual for creating AS blocks and OS faceplates for PCS7 V7.0: Programming instruction for blocks |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
10/26/2017 9:24 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by Kiiza is split to a separate thread with the subject How to create a structured tag for this block in WinCC v6.2.?. Best regards |
11/13/2017 3:38 PM | |
Joined: 11/17/2014 Last visit: 8/28/2023 Posts: 184 Rating: (0) |
Here is the other attachment |
Follow us on