10/25/2017 1:04 PM | |
Posts: 12 Rating: (0) |
hi I set up project in s7 1200 1212c and created one scada application in SIMATIC PC Station (HMI_RT_1 (Wincc RT Advanced). the ladder application i downloaded to 1212c and it is running fine. the scada application I saved and start run time on the pc . it is not running with cpu 1212c. showing error as incorrect access point/module configuration ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/26/2017 10:17:53 AMNew subject after splitting |
|
10/25/2017 1:08 PM | |
Joined: 5/12/2006 Last visit: 9/24/2024 Posts: 22371 Rating: (3012)
|
screen of the message? Do you check the PG/PC Settings in Windows Control panel? |
Follow us on