11/9/2017 3:12 PM | |
Posts: 4 Rating: (0) |
HI I have a problem regarding SIWAREX U WEIGHING MODULE ( 7 MH4950-2AA01), THE SUPPLY VOLTAGE TO LOAD CELL POWERING REGULATED VOLTAGE IS 07 VOLTS DC in place OF 6 VOLTS. is my module is faulty because it should be maximum 6 volts. ------------------------------------------------------------------------------------------ |
Last edited by: kapiln at: 11/9/2017 3:14:00 PMLast edited by: CS Moderator at: 11/9/2017 11:50:22 PMNew subject after splitting |
|
4/9/2018 2:05 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by AutoGen_380851 is split to a separate thread with the subject Measuring Range Exceeded . Best regards |
Follow us on