12/5/2017 8:49 PM | |
Joined: 7/20/2015 Last visit: 9/13/2024 Posts: 154 Rating: (27) |
Dear Experts. I am using step7 v5.5 sp4. I have a machine uploaded backup. I want to find out analog input and output address. I attach machine backup. For example i want to find out analog input and output address IW1120 and QW1120. Which is used at profibus station 11, How can i fint these address in given backup. Please help. AttachmentPrinting.zip (221 Downloads) |
Regards |
|
12/7/2017 5:01 PM | |
Joined: 7/20/2015 Last visit: 9/13/2024 Posts: 154 Rating: (27) |
Dear Rescobedo, dchartier, Piotr.M Thanks for reply, someone explain FC20 code, which is used in my uploaded backup. given below. AN #IN2 L #IN3 SD #IN2 BEC OPN DB 3 OPN DI [DBW 26] OPN #IN0 LAR1 P#20.0 M001: L DBW [AR1,P#0.0] L 0 ==I BEC L 0 L DBW [AR1,P#16.0] <>I = DBX 0.0 L DBW [AR1,P#18.0] LAR2 A M [AR2,P#0.0] JC M002 L 0 JU M003 M002: A DBX [AR1,P#3.7] = L 0.0 L DBD [AR1,P#2.0] L DW#16#FF7EFFFF AD SLW 3 LAR2 AN DBX [AR1,P#3.0] OPN #IN1 JC M004 L D [AR2,P#0.0] JU M005 M004: OPN #IN1 AN L 0.0 JC M006 L PIW [AR2,P#0.0] T W [AR2,P#0.0] M006: L W [AR2,P#0.0] ITD M005: OPN #IN0 L DBW [AR1,P#14.0] ITD +D M003: DTR L DBD [AR1,P#26.0] -R L DBW [AR1,P#22.0] ITD DTR *R L 1.000000e+002 /R L DBD [AR1,P#26.0] +R T DBD [AR1,P#26.0] AN DBX 0.0 JC M007 L DBW [AR1,P#16.0] SLW 3 LAR2 OPN #IN1 L DBW [AR2,P#0.0] OPN #IN0 ITD DTR L DBD [AR1,P#26.0] *R M007: L DBD [AR1,P#10.0] *R RND T DBW 10 L DBW [AR1,P#8.0] >I JC M008 TAK L DBW [AR1,P#6.0] >=I JC M009 M008: T DBW 10 M009: L DBW 10 L DBW [AR1,P#24.0] +I T DBW 10 L DBW [AR1,P#20.0] LAR2 AN M [AR2,P#0.0] JC M00a L DBW [AR1,P#0.0] SLW 3 LAR2 L DBW 10 OPN #IN1 T DBW [AR2,P#0.0] OPN #IN0 M00a: +AR1 P#30.0 JU M001 |
Last edited by: Sandeep Bakoliya at: 12/7/2017 5:12:06 PMRegards |
|
Follow us on