12/12/2017 11:17 PM | |
Posts: 7 Rating: (0) |
Hi I have a question, I have a Modbus TCP Project, each with a Modbus server for reading and writing. Furthermore, I would need help for referencing the IO values in the registers, I have a MOVE but it is not possible to make a move for each input eg E0.0 to E0.7 Not every input to make the move just one for all. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/14/2017 8:52:32 AMEdited text for better reading. Last edited by: Jen_Moderator at: 12/14/2017 8:55:04 AMNew subject after splitting |
|
12/13/2017 12:22 AM | |
Posts: 7 Rating: (0) |
thanks a lot huggy the problem is that i have to write directly what i have in input 1 to Holdingregister [1 ] and for all inputs so |
Follow us on