12/15/2017 11:49 AM | |
Joined: 1/4/2017 Last visit: 9/14/2022 Posts: 5 Rating: (0) |
Hello again, Now i am close to ready with everything . But I have some issues with the homing , I would like to do a basic homing, I have 3 sensors 1 top 1 bottom and one homing, but something is just wrong, first of all the reaction time is pretty slow when i reach the top i guess it is need to be turn back as soon as possible, but it takes around 3-5 sec and and the same in the other direction and when I try to activate the home sensor nothing happens, i try to find something about it in manuals, but there is no result yet, if you can suggest something what can help i will appreciate it or if you can show the settings it also can helps a lot. Best Regards Alex ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/18/2017 8:12:41 AMNew subject after splitting |
|
Follow us on