(0)| 1/5/2018 4:11 PM | |
|
Posts: 1 Rating:
|
Dear I have the same issue. The industrial network in our factory is SINEC-H1 and linked with #6 PLC S5-155 with WinCC 5.0+SP2. The process station linked to WinCC by CP1613 and CP143 at each PLC station. We want to replace one PLC station with S7-400 and ET200 and use the existing backbone network SINEC H1. What is the required - or the media converter to link the two systems and use the same SCADA WinCC 5.0+SP2. Attached is the drawing. Can any one help. ------------------------------------------------------------------------------------------ AttachmentProposal.pdf (237 Downloads) |
Last edited by: CS Moderator at: 1/7/2018 10:52:16 AMNew subject after splitting |
|
Follow us on