1/10/2018 5:29 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Please provide complete MLFB number of 1PH series motor or motor name plate photo snap so as to help you. |
1/10/2018 8:05 AM | |
Joined: 10/17/2007 Last visit: 9/17/2024 Posts: 4031 Rating: (353) |
Not sure what kind of hw config. are you using. post part# or simply post one picture of your system. some description must clear --SIMDRIVE 611U not SIMODRIVE U, 1ph7XXX, IS SPINDLE MOTOR, NEED the whole info. of motor # I attached possible encoder cable information, you can order from Siemens or other suppier from on line. (possible PM me to get more information from local ) cable # is 6FX8002-2AC31-XXXX Hope that helps Roberson de Souza
Attachment6FX8002-2CA31-1BA0_datasheet_en.pdf (648 Downloads) |
If you like my comments please |
|
1/24/2018 1:36 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by 07112066 is split to a separate thread with the subject how to replace the new encoder for motor 1PH7107-2NF30-0CJ0. Best regards |
Follow us on