2/2/2018 2:14 PM | |
Joined: 12/18/2014 Last visit: 9/19/2024 Posts: 33799 Rating: (4199)
|
Under Tools> Parameter VM Mapping, you must select the desired parameter of the block and assign an address, e.g. VW0. In the LWE Editor, on the corresponding page, insert the Block "Scale Time" (under Others > Scale Time) and set the parameters under the properties of the scale time. See attachment. AttachmentLOGO-LWE.zip (396 Downloads) |
This contribution was helpful to2 thankful Users |
2/2/2018 2:53 PM | |
Posts: 4 Rating: (1) |
Thank you very much! It worked out nicely in my example, now I'll try for the real project! |
This contribution was helpful to1 thankful Users |
2/7/2018 7:24 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by spygol is split to a separate thread with the subject How can parameterize a clock time and be able to see and edit it on the web page?. Best regards |
2/13/2018 11:49 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by MMMZZZ is split to a separate thread with the subject LWE - Is there any good way to put these VW-variable list of valuables into a JSON or XML for the desired API? . Best regards |
Follow us on