2/17/2018 8:23 AM | |
Posts: 6 Rating: (0) |
hello @Murof I have a question and I hope you can make me fully understand it. I read that WinCC advanced can be used for PC based single user system - and as far as I understood from that is that WinCC Advanced can be used for single PC only not two or three ... my question is, if I used winCC advanced to configure and two WinCC advanced RT license one two PCs (SCADA) and both PCs are connected with single PLC let's say S7-300 in a network so that System can be monitored and controlled through those two PCs would that work then? Thank you ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 2/19/2018 8:49:41 AMNew subject after splitting |
|
2/21/2018 7:41 AM | |
Posts: 6 Rating: (0) |
first of all let me thank you for your response. But as this would work why people tend to pay for client / server license? I can’t really figure that out. |
Follow us on