2/26/2018 1:38 PM | |
Joined: 1/1/2018 Last visit: 5/9/2020 Posts: 2 Rating: (0) |
Hi, We have HMI MP370, It is connected in network & send data to PC, Earlier Operating system of PC was windows XP, that time data send from HMI to PC was working ok, After changing Operating system of PC by 'Windows7 Enterprise', data transfer from HMI to PC is not working, how to configure 'HMI MP370 network setting' so that it can send data to PC which having operating system 'windows7 Enterprises' Thanks, Suhas ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 2/26/2018 2:39:49 PMNew subject after splitting |
|
2/26/2018 2:18 PM | |
Joined: 4/24/2006 Last visit: 4/25/2024 Posts: 8613 Rating: (1147)
|
Hello, Please have a look at the following links: How do you integrate an HMI operator panel into a local network? and Integrating HMI Operator Panels in TCP/IP Networks and access to a NAS or to a shared Windows folder Best regards, Wizard |
3/1/2018 1:12 PM | |
Joined: 1/1/2018 Last visit: 5/9/2020 Posts: 2 Rating: (0) |
Hi, Thanks for the information, I tried same, when connects PC having Windows XP, data transfer works ok, but when connects PC having Windows7 Enter, data transfer not works, I have doubt does MP370 supports windows7 Enter ? If no, then how to upgrade HMI MP370(windows CE Version3.0) ? Thanks, Suhas |
Follow us on