3/7/2018 4:13 PM | |
Joined: 2/26/2018 Last visit: 3/26/2024 Posts: 1 Rating: (0) |
Hi, I am working with s7-1200 plc. I tried to upload a program from s7-1200 1215dc/dc/dc with tia portal v14 and its showing an error " this blocks are editable with v13 only. So, again tried with v13 sp1 and the program was uploaded. When i try to download the modified program into that plc errors are occured like " firmware incompatibility online 4.2 and offline 4.1". What to do now pls give me solution. Thanks in advance ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 3/8/2018 2:27:24 PMNew subject after splitting |
|
3/9/2018 5:41 PM | |
Joined: 7/7/2010 Last visit: 5/3/2024 Posts: 14680 Rating: (2350)
|
If you configure your PLC hardware settings to allow the download as long as the PLC being loaded is "compatible" (even though part # or firmware may differ), you should change from error to warning. To get around this, I suggest factory reset the PLC, then (make the hardware configuration change to allow compatible differences) compile hardware / software and download again.
|
science guy |
|
Follow us on