5/30/2008 12:23 PM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating: (272) |
dear darius
thanks for your kind reply |
VANDE MATARAM..... |
|
6/16/2009 9:13 PM | |
Posts: 1 Rating: (0) |
Thanks Very Much I am a new user and this fixes my Issue. |
9/12/2012 9:51 AM | |
Joined: 4/24/2006 Last visit: 9/20/2024 Posts: 8742 Rating: (1168) |
Hello poojad, You want to use IW128. Here is some information about CPU: http://support.automation.siemens.com/WW/view/en/36816516/td The standard Proces image is 128 byte. (So you can use IW126, but not IW128) If you go to hardware configuration, you can double click on CPU and go to tab 'cycle/clock memory'. Here you can change the Proces image. Or use PIW128 in stead of IW128 Where and when do you need peripheral addressing? Best regards, Wizard |
This contribution was helpful to3 thankful Users |
9/15/2012 1:31 PM | |
Posts: 13 Rating: (0) |
Thank u for asking this question... Me too did the program in this manner... Now i corrected... |
5/5/2017 12:55 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by AutoGen_8148914 is split to a separate thread with the subject CPU 314C 2PN/DP, more addressing then MB0 to MB255. Best regards |
Follow us on