3/17/2018 5:26 AM | |
Posts: 8 Rating: (0) |
Dear Expert, I read at https://support.industry.siemens.com/cs/ww/en/view/11376409 that TP 700 comfort can connect with HL-L5100DN brother printer via USB/Ethernet and tested withWINCCV14. so I have a question: Is it possible to connect TP 700 panel with HL-L5100DN brother printer usingWINCCV13 Sp1? Thank a lot!
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/19/2018 7:28:35 AMNew subject after splitting Last edited by: Jen_Moderator at: 3/19/2018 7:33:17 AMOptimized link. |
|
3/18/2018 9:47 AM | |
Joined: 5/28/2008 Last visit: 9/9/2024 Posts: 4515 Rating: (839) |
Hello, As per info you already read in the mentioned pdf, I have checked the comptability tool for you and here's attached the result. It told us that with TIA V14 SP1, no additional driver required. No direct statement that with V13, it will or won't work. But I think you may need to install printer driver in this case. Try to install driver from the following link: AttachmentCompatibility tool - Version 2.2018.01.0 - Build - 20171220 03_34_17.pdf (522 Downloads) |
Last edited by: Jen_Moderator at: 3/19/2018 7:35:48 AMOptimized link. Ayman Elotaify |
|
Follow us on