3/20/2018 12:33 PM | |
Joined: 4/28/2017 Last visit: 3/14/2024 Posts: 149 Rating: (24) |
Dear All, I have prepared a simple File which has information about "How to configure Siemens SIRIUS SOFT STARTER". It may be useful to somebody who is having no experience in the soft starter. And, The Model in which I worked is "3RW40". But, Its common to all the Soft starter except some Over Load Limitation Parameters. This kind of starter parameters is very sensitive if you are in need of Protection against the load. Read the Document here beneath. Post your commands if you have any queries. AttachmentSIE_SOF_STATR.pdf (677 Downloads) |
Last edited by: Sanakiyen at: 3/20/2018 12:34:44 PMLast edited by: Sanakiyen at: 3/20/2018 12:35:22 PMLast edited by: Sanakiyen at: 3/21/2018 10:26:59 AMLast edited by: Sanakiyen at: 3/21/2018 3:30:04 PMNote: If this post did really help you, you may use the "Rate" button to express your support, Thank you. |
|
Follow us on