3/23/2018 3:26 PM | |
Posts: 1 Rating: (0) |
Good day Everybody. Does anybody know how to create ladder logic which can calculate a speed of a movement? CPU used for this purpose is CPU317-2 DP, and the movement is measured by using the resistor strip ( input signal is converted to 0-10 Volts ). I have tried several options to calculate the difference between "actual position" and "previous position" but the value has not been visible in the program when it was running online. How to measure the time between two events ( positions )? Best regards and many thanks. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/26/2018 8:05:35 AMNew subject after splitting |
|
Follow us on