3/29/2018 6:01 PM | |
Posts: 2 Rating: (0) |
Hello, I have a project with an existing project including a CPU 315-2 Profibus system. Recently I added a IM151-1 DP slave with power module and Siwarex CS module. The IM151-1 DP slave works and shows no problem in the hardware config. Also the calibration of the Siwarex CS module was successful (with Siwatool CS software). The problem is that I can't access the data, online in the buffer of the CPU I get a read/write error from the Siwarex CS address used in the FB42 block. Can somebody help me solving this problem? (I will add the project, the use of the FB42 is in FC10) Kind regards
AttachmentCross_co.zip (63 Downloads) |
Last edited by: ThomasBrondeel at: 3/29/2018 6:07:29 PMLast edited by: ThomasBrondeel at: 3/29/2018 6:08:33 PMLast edited by: ThomasBrondeel at: 3/30/2018 12:12:45 PMLast edited by: ThomasBrondeel at: 4/3/2018 12:31:08 PM |
|
5/8/2018 11:54 AM | |
Joined: 6/19/2017 Last visit: 5/2/2024 Posts: 7986 Rating: (163) |
New question published by alireza_ghaderi is split to a separate thread with the subject CPU 315-2 DP with IM151-1: Getting a fault after inserted 7 AI card HS 134-4gb52-0ab0. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on