Industry Online Support
Technical Forum
4/13/2018 12:15 AM | |
Joined: 3/11/2017 Last visit: 3/4/2024 Posts: 4 Rating: (0) |
Hello Frink, I use JOB 70 to transfer recipes from the IHM to the CLP. However depending on how long the bit that gives condition to the transfer is in state "1" the Tags of the Recipe are all in "0" state coincident with the time of the job mailbox acquisition cycle. The problem does not happen with Strings, only with Real and Time This does not happen in PLCSim. Any idea how I can heal this problem? Thank you! ------------------------------------------------------------------------------------------ AttachmentDownloads.zip (164 Downloads) |
Last edited by: Jen_Moderator at: 4/13/2018 12:12:10 PMNew subject after splitting |
|
Follow us on