4/17/2018 9:19 AM | |
Joined: 4/9/2015 Last visit: 7/18/2022 Posts: 11 Rating: (1) |
Hello everyone I'm experiencing some issues with my tia scout (4.4.0.11). The LAD/FDB editor is not opening when I try to open a program block. The problem appears to be identical as described in this patch: https://support.industry.siemens.com/cs/ae/en/view/109745779 Installation of this patch fails (see log txt). Note that i have no V4.5 of simotion scout installed, I do have the more recent V5.1.0.1 scout & tia scout installed. Any ideas? Thx Koen AttachmentPatch_SCOUT_TIA_V44_SCOUT_V45_Log.txt (488 Downloads) |
Last edited by: Jen_Moderator at: 4/17/2018 11:54:28 AMOptimized link. |
|
4/17/2018 9:43 AM | |
Joined: 4/9/2015 Last visit: 7/18/2022 Posts: 11 Rating: (1) |
Hey, Thx for the response! -Yes to the first question (V5.6 + HF1) -No to the second question (see attachment) Grz Koen |
4/17/2018 9:48 AM | |
Joined: 5/12/2006 Last visit: 9/25/2024 Posts: 22372 Rating: (3015)
|
Hello, have you also installes S7-Graph ? If yes which Version? Christoph |
4/17/2018 9:52 AM | |
Joined: 4/9/2015 Last visit: 7/18/2022 Posts: 11 Rating: (1) |
Yuppers, SIMATIC S7-GRAPH Professional 2017V5.6 V5.6.0.0_8.1.0.1 V5.6.0.0 Attachmentsoftware.txt (437 Downloads) |
4/17/2018 10:04 AM | |
Joined: 5/12/2006 Last visit: 9/25/2024 Posts: 22372 Rating: (3015)
|
Hello, ok this is not good. The S7 Professional 2017 install some newer Common Tools which used from Step7 and Simotion Scout / Simotion Scout TIA. The problem is that the old Scout /Scout TIA V4.4 is not compatible with the new versions. So you can do: Uninstall Simotion Scout V5.1 and Step7 Professional (include all packages from the Professional like s7-Graph) Install Step7 professional without S7-Graph (if you don't need it), then Scout V5.1 , then it should work. Open a support Request and report this to the Customer Support , it can be that some HF or Patch is available for this problem.
Christoph |
8/28/2018 6:33 PM | |
Posts: 8 Rating: (0) |
I had an almost identical problem, and I just wanted to post my solution in case it can be of use to someone in the future. I got the following response from Siemens tech support and it fixed the issue for me right away. ===================================================================== Please download and install HF5 for Step7 V5.6: https://support.industry.siemens.com/cs/us/en/view/109759316 Yes, I realize you reported a problem in Scout TIA, but I found a problem report from development that identifed the Step7 V5.6 as a potential source of the problem in Scout TIA, HF5 is supposed to correct it. ===================================================================== Good luck! |
This contribution was helpful to1 thankful Users |
8/29/2018 12:07 AM | |
Joined: 8/18/2014 Last visit: 9/21/2024 Posts: 59 Rating: (0) |
I had some problems too with V5.1.0.1 scout, but then I installed V5.2. Try to install this new version.
|
Follow us on