4/30/2018 10:17 AM | |
Joined: 7/5/2013 Last visit: 9/26/2024 Posts: 3114 Rating: (512) |
Dear Goedhuja, Configuration tool: WinCC flexible Standard Version 2005 SP1 or higher, see 6AV6643-0CB01-1AX1. But it says "WinCC xxx (TIA Portal): Yes", too. Maybe you have to download the HW-file for this panel, because for 10" panel it is shown the same, see 6AV6643-0CD01-1AX1. Regards, Frink |
Pi is exactly three! |
|
5/4/2018 12:03 AM | |
Joined: 3/19/2018 Last visit: 4/28/2024 Posts: 42 Rating: (0) |
Indeed that is what I want, juist to install SP1 On the v14.0. But can’t find this update to sp1 and how to... |
5/4/2018 6:08 AM | |
Joined: 5/12/2006 Last visit: 9/25/2024 Posts: 22372 Rating: (3015) |
WinCC V14 SP1 https://support.industry.siemens.com/cs/ww/en/view/109746074 Step7 V14 SP1 https://support.industry.siemens.com/cs/ww/en/view/109745153 Regards Christoph |
Follow us on