5/10/2018 1:19 PM | |
Posts: 10 Rating:
|
Hi I am trying to make a program similar to one called "speed control" to run my electric motor but in my case: - The speed is (20%,40%,60%,80%,100%) and can be choose from the list by using Up and down buttons(arrows). Exp: On display TDE we can see: numbers SPEED: 1- 20%, 2 - 40%, 3-60%, 4-80%, 5-100%.
To run the motor we have to by using arrows up/down choose number we want, for example "1" and press start button (input 1) - motor will run with 20% of the speed If we choose: "2" and press start button (input 1) - motor will run with 40% of the speed, etc. The program will be much more complicated cos there will be RPM meter and OFF DELAY timer too. I have got the timer circuit made already and that seems to be working ok. I will need make RPM meter - one impulse per rev (2-7RPM - quite slow) If You have any examples ideas for it I will be grateful Thanks Attachmentspeed control.zip (243 Downloads) |
5/10/2018 2:39 PM | |
Joined: 12/18/2014 Last visit: 9/7/2024 Posts: 33709 Rating:
|
For which LOGO! ? 0BA7? 0BA8.Standard? 0BA8.FS4? |
5/10/2018 2:59 PM | |
Posts: 10 Rating:
|
|
5/10/2018 3:40 PM | |
Posts: 10 Rating:
|
Yes no display I have TDE as well 6ED1055-4MH08-0BA0 and analog output too. |
5/10/2018 3:43 PM | |
Joined: 12/18/2014 Last visit: 9/7/2024 Posts: 33709 Rating:
|
The start button (I1): Is it an push button or a switch? |
5/10/2018 3:56 PM | |
Posts: 10 Rating:
|
Push button and arrows UP/DOWN (C1,C2) are on TDE to increase/decrease speed. |
Last edited by: lolos79 at: 5/10/2018 4:00:24 PM |
|
5/10/2018 7:09 PM | |
Joined: 12/18/2014 Last visit: 9/7/2024 Posts: 33709 Rating:
|
I created a program for you, see if you like it.
AttachmentSpeed_selection_0BA8.Standard.zip (275 Downloads) |
This contribution was helpful to
1 thankful Users |
5/10/2018 8:03 PM | |
Posts: 10 Rating:
|
This is great thanks very much !! |
This contribution was helpful to
1 thankful Users |
5/15/2018 6:46 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating:
|
New question published by lolos79 is split to a separate thread with the subject How can make it work that the last configuration will not be forgotten and still will be on the screen?. Best regards |
Follow us on