5/11/2018 1:51 PM | |
Posts: 3 Rating: (0) |
Is it possible to attach more than one button to the invisibility animation? I have a silo control program that has 4 ingredient options/silo and I would like to lock or make the other three invisible when one of them is pressed. So far I´ve only found a way to attach one button (or a tag) to the invisibility animation. I´m using Tia portal V13 with Wincc and step 7 and a Logo!8.0 plc with KTP 700 basic display. ------------------------------------------------------------------------------------------ |
Last edited by: Cosfoortti at: 5/11/2018 1:52:50 PMLast edited by: Jen_Moderator at: 5/14/2018 8:45:09 AMNew subject after splitting |
|
Follow us on