5/14/2018 9:13 PM | |
Posts: 10 Rating:
|
I updated my program. I have got few issues and few questions too I added docking button with make machine stop in certain loading position (sensore position), added rotating time setting etc: - Program works but RPM meter not ( I dont know why) - I need to stop unwanted persons to play with time and speed, so I need the password to change them. I read somewhere, tde can be used in two modes: admin and user (for user arrows, esc, enter will not work). Is that true and how can I do it? I think it will block access to tde settings, logo settings, logo selection, etc - When the tde is starting up first screen holds on date and time . How can I make it to go to first page instead of that? - Is there any chance to monitor how long machine (motor) is working from new. - The most important thing: When an admin set up the best configuration (time + speed) for a machine, I need to save it in the memory and if the machine will be turned off and on again, the last configuration will not be forgotten and still will be on the screen. Is any chance to do it? - Last thing - As I have got speed set now, maximum voltage on analog output can be 7V (7 RPM). How can I set 7 RPM but there will be 10V on output. That's all. English is my second language so I am very sorry for any spelling mistakes. Thanks ------------------------------------------------------------------------------------------ AttachmentSTS_mixer v1.zip (289 Downloads) |
Last edited by: Jen_Moderator at: 5/15/2018 6:46:37 AMNew subject after splitting |
|
5/14/2018 10:51 PM | |
Joined: 12/18/2014 Last visit: 9/7/2024 Posts: 33709 Rating:
|
Ha, ha, ha, that's not very little, that's a lot of problems and questions. The LOGO! the program works out on numbers of blocks. In your program, the block with the timer has a lower number than the block with the calculation. As a result, the measured time value is already cleared before the calculation takes place. I changed the block numbers and now it works. Switching from ADMIN to Operator only causes the LOGO! own menu is restricted. The operator can then, e.g. only the IP address in the menu, but can not change. He can also do the LOGO! via the menu no longer start or stop because the menu item is missing. If you want to know more, you should read the manual. But the keys are not locked. Would make no sense, the operator should actually be able to adjust setpoints. If you want to prevent this, you have to create yourself a password function in the program. I have programmed something like this before. Message texts are only displayed if they are activated. Your message texts are only activated as long as you press the associated F-key. For the simulation, you can set the F-keys under the block properties as a switch, but this has no effect on the real F-keys.
So you want to count the switch-on time of the two outputs? If so, then the LOGO! the block "hours counter" for this purpose. However, this only covers whole minutes. If the output is e.g. only turned on for a maximum of 59 seconds (or less), this is not detected. In that case you would have to program yourself an hour counter. In the "Counter" block of your setpoint generator, switch on the retentivity. You still need to amplify the output of the analog MUX, e.g. with an analog amplifier. Have I inserted into your program. AttachmentSTS_mixer v2.zip (250 Downloads) |
5/15/2018 6:28 PM | |
Joined: 12/18/2014 Last visit: 9/7/2024 Posts: 33709 Rating:
|
I created something for you. With F1 you can toogle between the RUN screen and the INFO screen. Press F2 to open the password screen. Here you enter the password. If the password is recognized as correct, the TIME screen and the SPEED screen are enabled. With F3 you can toggle between the TIME screen and the SPEED screen. The enabling ends after a time (10 minutes) or by pressing F2 again. The password consists only of numbers and is the ON value of the counter in the UDF "password", the OFF value of the counter is always password number + 1. Currently the password in the UDF is "618724" (ON value), the OFF value is then 618725. You ca change it, if you want. If you then make on the program a copy protection, the operator can not read it. The cursor keys for adjusting the setpoints are locked with the corresponding screen, they only change the setpoint if the associated screen is activated. Without enable by the password, there is no activation. AttachmentSTS_mixer_V3.zip (272 Downloads) |
5/15/2018 8:47 PM | |
Joined: 12/18/2014 Last visit: 9/7/2024 Posts: 33709 Rating:
|
You certainly have not included the UDF in the UDF library. Tools > Options > UDF |
5/15/2018 9:46 PM | |
Joined: 12/18/2014 Last visit: 9/7/2024 Posts: 33709 Rating:
|
Because the UDF has been updated, the calls in the password screen have been deleted. Only had to be inserted again. Edit: I have made to password to "111". AttachmentSTS Mixer V3.zip (298 Downloads) |
Last edited by: ixo65 at: 5/15/2018 9:49:44 PM |
|
Follow us on