5/18/2018 5:46 PM | |
Joined: 3/23/2018 Last visit: 12/7/2023 Posts: 16 Rating: (0) |
Hi all , I created a small logic which controles a compressor according to the feed back from air pressure transmitter. logic works fine. i also added a hours counter in the logic to show the Running hour,that also works fine,But problem is that when i want to modify the logic the Hours counter value should also start from Zero.Since i am a beginner can any one suggest any logic to solve this issue? I don't think that online editing is possible in Logo if i am wrong please correct me. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 5/22/2018 7:13:38 AMNew subject after splitting |
|
Follow us on