5/18/2018 7:31 PM | |
Joined: 7/15/2016 Last visit: 8/27/2024 Posts: 2 Rating: (0) |
Hi, I wonder if you ever used the OpenPCS7 within the OS Server station? I would like to do a test if possible within my laptop which is in this case the ES. Thus I create an OS Server station in the project and name it to my laptops name. add the SPOSA app in the OS Server config. Set the Ethernet as IE General and the IP address same as ES. Download or import to Station configurator. Seems fine so far. But I am not able to connect via OPC Scout locally. I assume it is because it does not allow me to set the path of the application to the same PC station. Is there a workaround? Thanks. ------------------------------------------------------------------------------------------ |
Last edited by: AutoGen_9313252 at: 5/18/2018 7:32:16 PMLast edited by: Jen_Moderator at: 5/22/2018 10:03:02 AMNew subject after splitting |
|
Follow us on