7/5/2018 10:53 AM | |
Joined: 8/3/2009 Last visit: 5/8/2024 Posts: 12909 Rating: (1646) |
Hello ssmanku1699 This should be no problem or also no other way of doing as with an integrated Ethernet Interface. If you have everything integrated in Step7 Project then the Netpro does the job for you if you use a manual connection then use the IP adress of the CP and the Slot ID of the PLC!! Use this one: https://support.industry.siemens.com/cs/ww/en/view/24109937 Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on