8/12/2018 11:03 AM | |
Joined: 5/6/2010 Last visit: 5/12/2024 Posts: 1965 Rating: (273) |
Hello Matty, I would suggest the follow:
Please look at the attachment, there is a "first" suggest. This tool is very helpful, because you have a part list and a interface to the Siemens Mall. regards AttachmentProject_Temp_20180812.zip (154 Downloads) |
This contribution was helpful to1 thankful Users |
8/15/2018 6:13 PM | |
Posts: 50 Rating: (0) |
Hi again, I have attached a quick birds eye view of where the machines are located and the locations of they want the HMI's. It seems i was slightly out on the distances (150-200m) but i have now measured the correct distances. Is this the way you would configure the network and if it is not, could you tell me the reasons why? i have no previous experiences with fiber networking so what other options have i got with the distances? The thermistor mounted inside the motor is a PTC/NTC KTY84 ( https://www.nxp.com/docs/en/data-sheet/KTY84_SER.pdf? ) So do i need an analogue input that reads 4-20mA? After putting a price to the directors they now only want the 8 anilox shafts and 8 print cylinder shafts monitoring so i now only need 16 inputs per press and 64 overall. do i keep the same CPU you first placed in your example? The 3 phase power modules, do i need them if i already have a 24vdc supply in the electrical container? Thanks again for your help, Matty G Attachmentmotor temperature.docx (169 Downloads) |
8/17/2018 8:32 AM | |
Joined: 5/6/2010 Last visit: 5/12/2024 Posts: 1965 Rating: (273) |
Hello Matty, here my suggest:
I hope you can see what I mean at the atteachment. I hope this is helpful for your challenge regards AttachmentTemperaure.zip (201 Downloads) |
Last edited by: Jen_Moderator at: 8/17/2018 11:27:06 AMOptimized link. |
|
This contribution was helpful to1 thankful Users |
8/17/2018 3:21 PM | |
Posts: 50 Rating: (0) |
Cheers! Unfortunately i cannot open the .tia file. it says (Not a valid path)? Cheers Matty G |
8/25/2018 10:33 AM | |
Joined: 5/6/2010 Last visit: 5/12/2024 Posts: 1965 Rating: (273) |
Hello Matty,
Hope this helps for the first time. regards |
Follow us on