8/16/2018 8:49 AM | |
Joined: 12/18/2014 Last visit: 6/17/2024 Posts: 33204 Rating: (4107)
|
I have created the program times according to your specifications. Start the simulation and let the actual value increase. Output Q1 is permanently on, since it is below 90. If the transition from 89 to 90 now occurs, it came a pulse for output Q1. However, it can not be recognized as an independent pulse since it only acts as an extension of the on-time of Q1. AttachmentKarthikk.zip (163 Downloads) |
This contribution was helpful to1 thankful Users |
8/17/2018 6:25 AM | |
Joined: 12/18/2014 Last visit: 6/17/2024 Posts: 33204 Rating: (4107)
|
The new Version.
AttachmentKarthikk_V2.zip (148 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on