12/28/2011 10:47 AM | |
Joined: 10/11/2006 Last visit: 5/13/2024 Posts: 5837 Rating: (790) |
Hello, you can use the data out of the configuration manual. Page 5-109. http://support.automation.siemens.com/WW/view/en/28687754 Table 5-18 Motor type 1FE1084--6WU11 Three--phase synchronous built--in motor 1FE1084--6WU11 Rated power PN kW 23 Rated speed nN RPM 1700 Rated torque MN Nm 130 Rated current IN A 45 Maximum current Imax A 90 Maximum rotational speed nmax RPM 7000 Rotor weight mRot kg Refer to Table 1-4 |
With best regards, |
|
Follow us on