10/25/2012 2:08 PM | |
Joined: 10/11/2006 Last visit: 4/18/2024 Posts: 5819 Rating: (787)
|
Hello enku, 1PH6103-4HH56 AC MAIN SPINDLE MOTOR, DC LINK 600 V 9.5 KW, 3000 REV/MIN, 30 NM SEPARATE VENTILATION, INCR. OPTICAL ENCODER, IP54, TERMINAL BOX, SIGNAL CONNECTOR WITH HTL ENCODER ROD431; TYPE IM B35 The detailed converter list I can not find in the data base. Only that motor but with other windings - G/F - but not H. Some values what I found in an other source: U=348V In=25A Pn=9,5KW nn=3000rpm nmax=7500rpm cosphi=0,75 f=102,6Hz encoder HTL 1024 S/R Temp. sensor KTY84-130 Alternativeyou could insert that motor in Sinamics via the mask foreign motor. Afterwards you can start a motor identification. Servo and vector mode is possible. If you have a position application you should use servo for e.g. a winder vector should be used. |
With best regards, |
|
6/23/2016 3:16 PM | |
Posts: 1 Rating: (0) |
Dear Gentlemen, I am looking for all technical data following motor: 1PH6163-4HZ56-Z It has na encoder H01 1024 S/R and I would appreciate if you could confirm if it is na Sin/Cos or TTL encoder and also the voltage supply range. Thanks |
Follow us on